Searching . . .

Related press releases

February 14, 2011

Vishay Intertechnology Releases New Series of Screw-Terminal Power Aluminum Capacitors With Long Life of 5000 Hours at +105°C and High Ripple Current to 34.8 A in 11 Case Sizes

December 01, 2010

Vishay Releases New Series of Screw-Terminal Power Aluminum Capacitors in Nine Case Sizes Ranging From 50 mm by 80 mm to 90 mm by 220 mm

September 16, 2010

Vishay Releases Industry’s First Surface-Mount Aluminum Capacitors to Combine Low Impedance Down to 0.035 Ω With High Ripple Current to 1.75 A, While Meeting IPC/JEDEC J-STD-020 Soldering Standard

July 29, 2010

Vishay Extends 140 CRH and 150 CRZ Series Surface-Mount Aluminum Capacitors with New Devices That Meet IPC/JEDEC J-STD-020 Soldering Guidelines

July 15, 2010

Vishay Releases New Series of 4-Terminal, Snap-In Power Aluminum Capacitors With 10,000-Hours Useful Life in Case Sizes From 35 mm by 50 mm to 45 mm by 100 mm

January 20, 2010

Vishay Enhances 101/102 PHR-ST Screw-Terminal Power Aluminum Capacitors With Three Large Case Sizes to 90 mm by 220 mm, and 13-mm Terminals

October 30, 2009

Vishay Releases New 142 RHS Series of Radial, 105 °C Aluminum Capacitors With Capacitance Values up to 22,000 μF at 10 V and Ripple Currents to 3100 mA at + 105 °C

January 23, 2009

Vishay Releases New 146 RTI Series of Radial, High-Temperature, Low-Impedance Aluminum Capacitors With Z as Low as 18 mΩ, Capacitance Values up to 6800 μF, and Ripple Currents to 3200 mA at +125 °C

November 05, 2008

Vishay Releases New ECL Series of SMD Aluminum Capacitors With Z as Low as 90 mΩ, High Capacitance Values up to 1500 μF, and High Ripple Currents to 670 mA

August 01, 2008

Vishay Extends 140 CRH Series of SMD Aluminum Capacitors to Provide High Capacitance Values up to 1000 μF, High Ripple Currents to 900 mA at 125 °C, and Low ESR Down to 90 mΩ

July 09, 2008

Vishay Extends 150 CRZ Series of SMD Aluminum Capacitors to Provide Z as Low as 60 mΩ, Capacitance Values up to 2200 μF, and Ripple Currents to 1007 mA at +105 °C

April 26, 2006

Vishay's New Aluminum Capacitors Achieve Maximum Impedance at 100 kHz That Is as Low as 0.10 Ohms in RoHS-Compliant, Lead(Pb)-Free, Surface-Mount Package

April 26, 2006

Vishay's New RoHS-Compliant SMD Aluminum Capacitors Enable Operation up to 125 °C and Lead (Pb)-Free Soldering

February 10, 2006

New Vishay 093 PMG-SI Aluminum Capacitors Achieve 2,000 Hours Rated Useful Lifetime at +85 °C

November 11, 2002

Miniaturised ultra-long-life elcaps with green electrolyte save space in power applications

July 04, 2001

BCcomponents welcomes newest addition to family of snap-in capacitors

May 15, 2001

157 PUM-SI miniature snap-in electrolytic capacitor gives longer life at reduced cost

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword
Useful Links