Introduction
For proper bonding of strain gages and
temperature sensors, the workpiece surface must be
chemically clean and totally free of contaminants
before applying the adhesive. Recommended surface
cleaning procedures for all common structural
materials are described in Micro-Measurements
Instruction Bulletin B-129,
Surface
Preparation for Strain Gage Bonding
.
In the case of steel and aluminum parts with
finish-machined or formed surfaces, the surface
cleaning procedure can be summarized briefly as
follows:
- Removal of oily contaminants with a solvent
cleaner. Note: Immersion of the workpiece in a
degreaser is, by itself, inadequate; and, if done
as a preliminary step, must be followed by
cleaning with an uncontaminated solvent (one
which is never returned to the container or
otherwise reapplied after contact with the
workpiece).
- Light abrasion in the presence of a mildly
acidic wash, to dislodge and remove oxides and
mechanically bound contaminants.
- Thorough surface scrubbing with an alkaline
solution, to finish the cleaning process and
leave the surface at the appropriate pH level for
optimum bonding.
When the cleaning procedure is performed
strictly according to the instructions in Bulletin
B-129, and when the proper high-quality cleaning
agents are used, the surface will be left in a
condition best suited for bonding.
Described in these listings is a complete
assortment of M-Prep cleaning supplies, compounded
and selected specifically for surface preparation
in the installation of strain gages and temperature
sensors.
Page 1 of 5
|