|
Digital Signal
Processing
|
(...continued)
Like an analog filter, the digital filter is
selected on the basis of which frequencies in the
signal are to be retained and which are to be
rejected. Low-pass filters, the most common type, are
designed to allow signal components from 0 Hz (dc) to
some nonzero passband frequency,
, to pass essentially unaltered. The filter
does introduce a series of small positive and
negative deviations from the actual signal in the
passband. When this "ripple" exceeds a
certain amount, typically 0.01 dB, it defines the
passband frequency. For frequencies in the transition
band between the passband frequency and higher
stopband frequency, the signal is increasingly
attenuated. When the attenuation reaches a certain
level, typically in the vicinity of 95 dB, it defines
the stopband frequency of the digital filter.
When using digital filters, the user should pay
attention to both the stopband and the transition
band. In some cases, particularly those with lower
passband frequencies, the transition band may be as
great as, or even greater than, the passband itself.
(continued...)
Page 7 of 24
|
|