|
Digital Signal
Processing
|
(...continued)
In the simplest of terms, the throughput rate is
little more than an indication of how much digital
data a specific combination of hardware and software
can acquire per unit of time. At the instrumentation
level, it is primarily controlled by the number of
analog-to-digital converters (ADC's) being used
in the system, and the rate at which the analog
signals being measured can be sampled and digitized.
The useful throughput rate of the overall data
acquisition system, however, is typically much slower
because of such things as (1) the need for
oversampling to eliminate aliasing in dynamic
signals, (2) the presence of bottlenecks in the
communications link between instrumentation and
computer hardware, and (3) limitations in the rate at
which software can acquire, reduce, store, and/or
present the digital data.
A calculation of throughput also requires knowledge
of how the instrumentation hardware acquires the
data. The simplest approach is to
sequentially sample
each data channel in the system at fixed intervals.
System 4000, the original Vishay Measurements Group
data system, acquires data in this fashion, using a
single ADC at a throughput rate of 25 or 30 samples
per second (depending upon the frequency of the mains
power).
(continued...)
Page 10 of 24
|
|