Digital Signal Processing
|
|
Time Skewing
Data acquired from various channels are often
functionally related. In stress analysis work, for
example, three separate channels might provide strain
data from the three grids of a strain gage rosette,
which are used together to calculate principal
stresses and strains. In this case,
when
the measurements were made is important if the three
signals vary with time. When such signals are sampled
sequentially, the resulting data are all taken at
different times, and are said to be skewed. The
errors produced by this skewing depends upon the
nature of the signal, the scanning interval (inverse
of the scanning rate) and the number of intervals
between the sampling of any two data points.
For sinusoidal signals with sequential sampling, the
worst-case errors will occur as the signal is
crossing through the inflection points. At these
points, the maximum frequency that can be sampled
without any
detectable
skewing (signal change of 1 LSB, or less, of the
full scale signal over a single scanning interval) is
a function of the sampling rate and the number of
"bits" into which the ADC digitizes the
full-scale signal. These frequencies are a few hertz
at best, even for relatively high sampling rates.
And, of course, the situation worsens as the number
of intervals between data points increases.
(continued...)
Page 18 of 24
|
|