(continued...)
Skewing errors greater than 1 LSB of full scale are
detectable and, as shown below, the measurable
frequency range is increased moderately if the
accompanying errors are acceptable.
Maximum frequencies that can be sampled at
various skewing error levels.
Of course, all skewing errors can be virtually
eliminated by using a digital data system, like
System 6000, that features
simultaneous sampling of all signal channels.
In these systems, the maximum time difference
between samples is typically in the nanosecond range,
such that skewing errors for all measurable frequency
ranges are undetectable.
Page 19 of 24
|