Installing Gages With Option
P
|
|
Strain Relief
Before unsecuring the cable bundle, it is
recommended that strain relief loops be provided in
both the cable and jumper wires. Form these loops
over the handle of a dental probe or rod of similar
diameter. The jumper-wire loop, which should lie in
the plane of the specimen, is usually held in place
by the protective coating. The cable loop, which
should remain upright, is usually located outside the
coated area.
M-LINE 3145
RTV
silicone rubber can be used as a cable anchor.
After the cable has been properly anchored, the
remainder of the bundled cable can be unsecured and
routed to the strain gage instrumentation. If a cable
extension is added, remember that it should be
attached by soldering. Alligator clips, twist caps,
and most other mechanical connections should be
avoided when making electrical connections within
strain gage circuits.
Gages supplied with Option P can be installed
readily with these techniques in most applications.
Should you have any questions about your particular
application, our
Applications
Engineering
staff here at the Vishay Measurements Group are
always ready to assist you.
Page 6 of 6
|
|