Mechanical Connectors
in Strain Gage Circuits
|
Page 1 of 3
A question that often arises, especially for
short-term strain gage measurements, is: "Can I
use mechanical connectors (screw-type, etc.) to
simplify connecting and disconnecting strain gages in
my instrument circuit?"
As for many other simple questions, there is no
simple answer to this one. In general, however, it is
preferable to use as few mechanical connections as
possible in any strain gage circuit. This is because
mechanical connections are potentially less stable in
joint resistance than soldered connections. When such
an answer is given, the next question is apt to be:
"But what about my strain gage instruments? All
of them are equipped with binding posts or other
types of mechanical connectors." True enough.
The connectors are there for the convenience of the
instrument user, but these are carefully chosen for
the intended purpose, and are often gold-plated or
gold-flashed to minimize and stabilize the contact
resistance.
It is always necessary to keep in mind the
relatively small resistance changes involved in
strain gage measurements. For a uniaxial working
stress of, say, 30 000 psi (207 MPa) in steel, the
strain level is 1000 microstrain. With a 120-ohm gage
(G.F. ~ 2.0), the strain-induced resistance change is
only about 250 milliohms. Under these conditions a
5-milliohm change in contact resistance will cause an
indicated
zero-shift
of some 20 microstrain -- enough to alarm a careful
practitioner. Yet contact resistance changes of this
magnitude can be caused by an oxidized connector
contact surface or by a poorly terminated
leadwire
. Even changing the insertion depth of the stripped
end of the leadwire into the connector can produce a
measurable zero-shift. With AWG #26 wire (0.4 mm
dia.), for instance, changing the insertion depth by
as little as 0.3 in (~8mm) when reconnecting the wire
will offset the zero by close to 5 microstrain.
(continued...
) |
|