Strain Gage Measurements on
Plastics and Composites
|
Plastics and Composites as Mechanical Test
Materials
In terms of experimental stress analysis, one of the
more significant differences between plastics and
metals is certainly in the basic mechanical
properties such as the modulus of elasticity. As
illustrated below, elastic moduli for plastics are
often two or more orders of magnitude lower than
those for metals. A practical consequence of this
difference is that measured strains on plastic test
objects tend to be considerably larger than on
metals, and can readily exceed 1 percent. The
relatively high-elongation strain measurements in
such cases can place special demands on strain gage
bonding and wiring procedures.
Order-of-magnitude comparison of
room-temperature and elastic modulus -- selected
materials versus 1018 steel. [ (1)T300/5208
graphite/epoxy; (2) Scotchply1002 glass/epoxy;
(Subscripts 1, 2 denote fiber and transverse
directions, respectively). (Ref.
3
) ].
Another potentially significant effect of the lower
elastic modulus -- and one that is less amenable to
user alleviation -- is that the presence of the
installed strain gage may, at least locally,
reinforce the test material. Perhaps indicative of
the state of the art in strain measurement on
plastics is the dearth of published data on
reinforcement effects. There are indications,
nevertheless, that reinforcement by the gage can lead
to very large measurement errors, particularly for
the lower-modulus plastics. (Ref.
1
and
2
)
(
continued ...
)
Page 5 of 32
|
|