Strain Gage Measurements on
Plastics and Composites
|
Strain Gage Selection
Beyond the usual criteria for gage selection
suitable to the strain-measurement task (i.e.,
single-element gage versus rosette, gage length,
strain range, operating temperature, etc.), the gage
resistance can be an important factor because of the
characteristically low thermal conductivities of the
test materials. High-resistance gages (350 ohms or
greater) are generally preferable to minimize heat
dissipation; but, in any case, the combination of
gage resistance, grid area, and excitation voltage
(grid power density) should be low enough to avoid
the instability caused by a sensible temperature rise
in the gage (Ref.
7
). For any given gage installation, the threshold of
instability can be established quite easily by
starting with a very low excitation voltage and
observing the (zero-strain) gage output while
gradually increasing the voltage. When using strain
gage rosettes, the single-plane rosette is preferred
over the stacked variety because of better heat
dissipation characteristics and less tendency for
reinforcement. These recommendations for dealing with
the self-generated heat in a strain gage assume
continuous gage excitation since this mode of
operation is employed in most contemporary
instruments. Heat generation in the gage can also be
minimized with pulsed gage excitation, if suitable
instrumentation is available.
Although the gage length is normally selected for
compatibility with the test-specimen geometry and the
expected strain distribution, other considerations
are also involved when making strain measurements on
plastics and composites. One of these, of course, is
grid power density, since the grid area commonly
increases with gage length. Another is that gages of
1/8 in (3 m/n) length or greater usually offer better
performance in terms of stability and strain range.
Additionally, with reinforced plastics, it is
imperative that the gage length be large with respect
to the dimensions of the underlying inhomogeneities
in order to obtain any meaningful strain
measurements.
(
continued ...
)
Page 16 of 32
|
|