Measurement of Force, Torque,
and Other Mechanical Variables With Strain
Gages
|
Installed Gage Resistance Test
Among its other capabilities, the
Model 1300
provides for convenient, precise measurement of the
gage resistance after installation. The instrument
indication is displayed as the percent deviation from
the nominal gage resistance, with full-scale ranges
of either 5% or 1%. Since Micro-Measurements strain
gages are manufactured to tightly controlled
tolerances on gage resistance, the magnitude of the
resistance shift due to installation provides a very
sensitive index to certain aspects of gage
installation quality. Shifts in gage resistance
during installation should not ordinarily exceed 0.5%
when using room-temperature-curing adhesives. With
elevated-temperature-curing adhesives, on the other
hand, the resistance shift may be greater due to the
thermal stress in the gage after return to room
temperature from the adhesive curing temperature. The
magnitude of the shift depends on the curing
temperature, the materials involved, and other
variables, but should never exceed 2%, and should be
uniform among identical gage installations to within
about 0.5%.
Excessive resistance shifts are usually indicative
of one or more flaws in the gage installation - poor
installation technique, questionable solder
connections, damage to the gage grid, leadwire
damage, etc. A unique feature of the Model 1300 is
that the completely wired strain gage can be
connected to the instrument in a 3-wire circuit, just
as it would be to a strain indicator. Thus, when the
Model 1300 is used in its deviation mode, the effect
of the normal resistance in matched leadwires is
automatically canceled, and the instrument will
therefore detect resistive faults not only in the
gage, but also in the leadwires and solder joints.
(continued...)
|
|