Remote Sense
|
Page 1 of 4
Remote sense or, more correctly, remote sensing
of excitation voltage, is commonly recommended for
use with precision, commercial transducers to prevent
leadwire resistance changes (due to changes in either
temperature or length) from affecting transducer
span, or sensitivity. This feature is less frequently
used with "homemade" transducers, and is
seldom used in strain gage test applications.
Transducer Applications
Leadwire attenuation presents a potentially
significant error source in transducers utilizing a
Wheatstone bridge circuit. The leadwires represent a
parasitic resistance, and a portion of the excitation
voltage intended for the bridge circuit is dropped in
the leadwire system, reducing the voltage actually
present at the transducer, and effectively reducing
the transducer sensitivity. If the temperature
remains constant during the setup and measurement
process, then correctly applying shunt calibration,
or a physical calibration of the transducer, is all
that is necessary to correct for the effects of
leadwire attenuation.
However, if the temperature of the leadwire system
changes during the measurement process, the
resistance will change correspondingly, changing the
amount of attenuation, and again resulting in a
calibration error. The resulting error is typically a
fraction of one percent, but with commercial
transducers, which demand the highest possible
accuracy, or when attempting to obtain the best
possible performance from a homemade transducer, even
that small error may not be acceptable. In those
instances, if the measuring instrument is provided
with remote sense capability, the error can be
effectively eliminated.
|
|