Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

New Dual-Channel LITTLE FOOT® TSOP-6 Cut MOSFET Count in Half For Load Switching in Cell Phones and Notebook PCs


LITTLE FOOT
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

MALVERN, PENNSYLVANIA - December 10, 1999 - A family of dual power MOSFETs in the TSOP-6 package, including the industry's first device rated for operation at 1.8 V, was released today by Vishay Intertechnology, Inc. Compared to previous-generation TSOP-6 devices from various suppliers, on-resistance for these new LITTLE FOOT® devices has been reduced by as much as 61%, making them a compact replacement for larger packages or multiple SOT-23 power MOSFETs in cell phones, notebook computers, digital cameras, pagers, and many other space-constrained electronic systems.

The four devices released today by Vishay Siliconix include two dual p-channel devices offering designers a choice of a P20-V breakdown voltage with 200 milliohms on-resistance at P4.5-V gate drive (Si3909DV) or an P8-V breakdown voltage with 125 milliohms on-resistance at a P4.5-V gate drive and 265 milliohms on-resistance at a P1.8-V gate drive (Si3905DV). The dual n-channel Si3948DV offers on-resistance of 105 milliohms, while the n- and p-channel Si3552DV provides n-channel on-resistance of 105 milliohms and p-channel on-resistance of 200 milliohms at a 10-V gate drive.

Target applications for the new devices are load switching in cell phones and mobile computing products and driving small motors in hard disk drives, camcorders, and minidisk players.

Samples and production quantities of all four new LITTLE FOOT TSOP-6 power MOSFETs are available now, with lead times of 8 to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword