English   日本語 (Japanese)   简体中文 (Chinese)   
VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoApplicationsCompany Info
Company Info:Press Room:2000 Releases:High Luminous Flux LEDs
For more information:
Media contact:  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233   Fax:  1.650.618.1512   E-mail:  bob.decker@wallstcom.com
 

High Luminous Flux LEDs Serve Automotive Lighting and Road Sign Applications: Vishay TELUX™ Series Is a High Luminous Flux LED in Full Color Range

MALVERN, PENNSYLVANIA - May 18, 2000 - A new family of high-intensity LEDs for roadside and automotive traffic signal applications was announced today by Vishay Intertechnology, Inc. The new Vishay Telefunken TELUXTM LEDs feature a full color range of devices with a wide viewing angle and high luminous flux for vehicle brake lights, taillights, and turn signals, as well as traffic signs, outdoor message panels, and warning lights.

A new family of high-intensity LEDs for roadside and automotive traffic signal applications was announced today by Vishay Intertechnology, Inc. The new Vishay Telefunken TELUXTM LEDs feature a full color range of devices with a wide viewing angle and high luminous flux for vehicle brake lights, taillights, and turn signals, as well as traffic signs, outdoor message panels, and warning lights.

Offered in red, yellow, true-green, blue-green, blue, and white versions, the new TELUX LEDs are packaged in a clear, industry-standard 7.62 mm square package optimized for maximum light output. Luminous flux for the new devices ranges from 650 mlm for the white TLWW 7600 to 2000 mlm for the red TLWR 7600 at +85°C Tamb. Designed to yield a precise and homogeneous spatial radiation pattern, the TELUX lens allows the use of fresnel optics or parabolic reflectors with consistent results. Two integrated package slots support direct assembly of light guides, reflectors, and external lenses.

"High luminous flux red and yellow LEDs are already popular solutions for automotive applications such as central high-mounted stop lights and turn signals," said Thomas Pakull, Product Marketing Manager at Vishay Intertechnology. "The new TELUX family is the first to combine high-end technologies, an industry standard package, and a full range of colors, which will greatly enlarge the universe of target applications for this device type."

The white TLWW 7600 LED, for example, can be used as a power- and space-efficient replacement for small incandescent lamps. The red TLWR 7600 and yellow TLWY 7600 meets SAE and ECE requirements for automotive red applications and can be used as a direct replacement for HPWA LEDs (Superflux) from Hewlett-Packard, while the blue-green TLWBG 7600 is recommended for green traffic signals, with a typical wavelength of 505 nm. All TLWx7600 devices are designed to perform in direct sunlight at high ambient temperatures and are built on the brightest state-of-the-art LED technologies,AllnGaP and InGaN.

Samples of the new TELUX LEDs are available now. Production quantities are available, with lead times of 2 to 3 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TELUX is a trademark of Vishay Intertechnology, Inc. All other trademarks are the property of their respective owners

 
LEDs
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2010 releases
2009 releases
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Terms and Conditions of Sale
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account