Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

New Oscillators From Vishay Combine 3.3-V Input Voltage With Frequency Range to 70 MHz


oscillators

Products mentioned:

XO-523 XO-543
XO-523
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

MALVERN, PENNSYLVANIA - June 9, 2000 - A pair of clock oscillators featuring a 3.3-V input voltage and a1-MHz to 70-MHz frequency range was announced today by Vishay Intertechnology.

A pair of clock oscillators featuring a 3.3-V input voltage and a1-MHz to 70-MHz frequency range was announced today by Vishay Intertechnology.

The new Vishay Dale devices feature TTL and HCMOS compatibility, plus a tri-state feature that allows the output to be placed into a high-impedance state. Both standard and industrial temperature ranges are available with two through-hole hermetically-sealed package options: 14-pin DIP (XO-543) and half-size 8-pin DIP (XO-523).

The new oscillators will provide clock signal sources for digital ICs and microprocessors in low-power applications including computers, portable peripherals, and communications equipment. Typical input currents for the XO-543 and XO-523 rangefrom 10 mA to 30 mA, with rise and fall times of10 ns maximum. A ±100-ppm frequency stability over operating temperature range is standard, with ±25 ppm and ±50 ppm also available

"The addition of these new oscillators to the Vishay product line broadens our frequency control products offering and thus the options available to designers, " said Mike Husman, Director of Product Marketing, Inductors, Thermistors, Crystals, and Oscillators.

Samples and production quantities of the XO-543 and XO-523 are available now, with lead times of 8 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword