Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This BCcomponents product press release (excluding the datasheet links and paragraph on Vishay) originally appeared on the former BCcomponents Web site.

BCcomponents at forefront of polypropylene film capacitor technology


Capacitor

Products mentioned:

MKP 338 X1
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

October 3, 2000 — BCcomponents, one of the world's largest manufacturers of passive components, today announced an important extension to its highly successful MKP338 X2 series - the MKP338 1 X1 440 Vac series, intended for use in general industrial applications as X2 or X1 interference suppression film capacitors.

BCcomponents has one of the largest product portfolios in the passive component industry. By further extending its product range, the company demonstrates its commitment to becoming the complete solutions provider for all passive component needs.

The MKP338 1 440 Vac series has the benefit of small dimensions and an increased rated voltage of up to 440 Vac, making it suitable for use in 3 phase applications demanding higher rated voltages in X2 or X1 class film capacitors. The series allows a capacitance value of up to 1 μF, with a pitch size of up to 27.5 mm.

“With the introduction of the 338 X1 440 Vac, BCcomponents is offering an even wider range of film capacitors for interference suppression applications,” said Linda Geeraerts, international product marketing manager, interference suppression capacitors, BCcomponents. “Once again BCcomponents is at the forefront of polypropylene film capacitor technology.”

The smaller size of the 338 1 440 Vac series, which is smaller than similar types on the market, gives designers the ability to significantly reduce the size of end products. Safe for use at temperatures as high as 105 °C and certified to all international safety approvals, including IEC 384-14 2nd edition / EN 132400 and UL1414, the new series can safely be used in equipment in all worldwide markets.

The 338 1 440 Vac series is supplied either loose in box, taped on ammopack or on reel. Customised versions are available on request. Datasheets and design-in support are also available and can be found on this website.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword