|
For more information: New Vishay Siliconix Battery Charger IC Works with All Common Battery Types, Offers the Smallest Footprint Solution on the Market for Cell Phones, PDAs, and Other Handhelds
SANTA CLARA, CALIFORNIA -March 23, 2001-A new microprocessor-controlled battery charger IC offering the industry's smallest footprint solution for this application - and eliminating the need for several external components - has been announced by Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH). Offered in a small-outline TSSOP-16 package with a 1.2-mm height profile, the new Si9731DQ works with system microprocessor or microcontroller of cell phones, PDAs, and other handheld appliances to provide a complete, chemistry-independent battery charger solution. The Si9731DQ uses two internal power MOSFETs to provide trickle charging or fast charging depending on battery voltage at the beginning of the charge cycle. If battery voltage is below 3.4 V, the Si9731DQ detects the voltage from an ac adapter and initiates trickle charging until the battery voltage reaches a sufficient level to wake up the system microprocessor. Once activated, the microprocessor disables trickle charging and enables PWM-controlled fast charging via the Si9731DQ. Both the trickle-charge and fast-charge MOSFET components of the Si9731DQ provide bidirectional current blocking on the off state, eliminating the need for an external Schottky diode. For maximizing the charge capacity of lithium ion batteries, the Si9731DQ integrates a precision reference and error amplifier to provide constant-voltage-mode charging to a 4.1-V or 4.2-V termination with 50-mV accuracy. Since it uses a pulse charging technique with short on-times and long off-times, power dissipation is kept to a minimum, but unlike any competing solution, no external inductor is required. The Si9731DQ typically draws just 1 mA of current in normal mode and a maximum of 1 mA of current in shutdown mode - an order of magnitude improvement over competing solutions. Because the Si9731DQ is microprocessor controlled, it gives designers maximum flexibility - allowing the same IC to be used for lithium ion or nickel battery designs, different charger types, different charging algorithms, and different power management architectures. As for power efficiency, the closest competing solution draws eight times the current in normal mode and 12 times the current in shutdown mode. The Si9731DQ can be used in conjunction with a regulated or unregulated external dc power source, including most low-cost wall adapters rated from 4.5 to 12 V. Samples of the Si9731DQ are available now. Production quantities are available now with lead times of 10 to 12 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |