|
For more information: New Power MOSFETs Are PWM Optimized for Line-Powered Synchronous Rectification Applications: Include Industry-First 12-V Device
SANTA CLARA, CALIFORNIA-March 30, 2001-Two new LITTLE FOOT® power MOSFETs for dc-to-dc converter circuits, including the industry's first PWM-optimized n-channel device with a 12-V maximum breakdown voltage rating, were released today by Siliconix incorporated (NASDAQ NMS: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH). Both new devices are intended for synchronous rectifier applications, serving low voltage outputs in dc-to-dc converters for desktop computers, network or routing cards, stand-alone power supplies, and other line-powered systems where a low-voltage microprocessor is needed. Until now, power MOSFETs optimized for synchronous rectification were available only in voltage ratings of 20 V or greater, sometimes diminishing efficiency and increasing heat generation when used in low-voltage products. The new Vishay Siliconix Si4838DY, with its 12-V VDS, breaks this barrier and offers a 40% overall performance improvement over any comparable device - with a maximum on-resistance of just 3 mΩ and a typical gate charge of 40 nC. For applications where more headroom is required, Siliconix is offering the new Si4876DY, a 20-V device with 5-m Ω on-resistance and Qg of just 55 nC - specifications which represent a 10% overall improvement compared with any competing device on the market. In many cases, supply currents require paralleling of synchronous rectification circuits, and many boards are stacked up. This means that the benefits offered by these new LITTLE FOOT devices are multiplied and therefore very significant. Overall performance for purposes of comparison is defined as the product of on-resistance times gate charge, with a lower score being better. Supply voltages are getting smaller, and lower-voltage synchronous rectifiers are required to prevent power from being wasted. The low on-resistance/gate charge product of these new devices means that converters can run at higher frequencies or with lower conduction and switching losses. That means more efficient use of power, less heat generated, and smaller space requirements. Offered in the LITTLE FOOT SO-8 package, samples of the Si4838DY and Si4876DY are available now. Production quantities will be available in January 2001, with lead times of 8 to 10 weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |