Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Industry's First Thermally Enhanced LITTLE FOOT SC-70 Power MOSFETs Deliver Threefold Improvement for Thermal Resistance, Feature ESD Protection to 2000 V


thin film
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

SANTA CLARA, CALIFORNIA-June 22, 2001-Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH) has announced that it is shipping a new series of LITTLE FOOT® SC-70 power MOSFETs for which thermal resistance has been reduced to the lowest level ever achieved for this package type.

The first thermally enhanced SC-70 power MOSFETs on the market offer package thermal resistance of 35®C/W for single-channel devices and 80®C/W for dual-channel devices, a respective improvement of 67% and 73% compared with the previous state of the art and similar to the larger TSSOP-8 package. This lower thermal resistance increases power dissipation to a maximum of 1 W in the single-channel SC-70 package, or allows the device to run cooler. Lower thermal resistance also contributes to the reduced conduction losses provided by these devices, in which rDS(on) is 25% or more lower than in standard SC-70 equivalents, extending lithium ion battery power.

The new LITTLE FOOT SC-70 devices, which measure just 2 mm by 2.1 mm with a 1-mm height profile, are aimed at small- to medium load switching, power amplifier switching, and level shifting applications in cell phones, pagers, PDAs, and other handheld devices. ESD protection prevents malfunction when the new devices are used in portable systems with attachable/detachable accessories such as SIM cards, Bluetooth adapters, IrDA adapters, MP3 adapters, and cable connections to other portable equipment.

Eight devices in the thermally enhanced LITTLE FOOT SC-70 were released, including single, dual, and complementary n-channel and p-channel versions with breakdown voltages of 12 V, 20 V, and 25 V. On-resistance at a ±4.5-V gate drive ranges from 70 mΩ for the single n-channel Si1410EDH to 490 mΩ for the dual p-channel Si1913EDH. All eight devices are rated for operation at 1.8 V for low supply voltages as well as at 4.5 V and 2.5 V. Maximum current handling ranges from 3.7 A for the Si1410EDH to -1 A for the Si1913EDH.

Samples and production quantities of the new thermally enhanced LITTLE FOOT SC-70 devices are available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

LITTLE FOOT is a registered trademark of Siliconix incorporated.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword