Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This BCcomponents product press release (excluding the datasheet links and paragraph on Vishay) originally appeared on the former BCcomponents Web site.

BCcomponents welcomes newest addition to family of snap-in capacitors


Capacitor

Products mentioned:

197 PGP-SI
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

July 4, 2001 — BCcomponents today launches a new addition to its popular family of snap-in aluminum electrolytic capacitors, the 197 PGP-SI.

The 197 PGP-SI is a general-purpose power capacitor targeting consumer applications such as audio-visual equipment, domestic appliances and PCs.

“The 197 PGP-SI is ideal for those market products that have set life expectancies, such as the consumer electronics market,” said Roger Appelo, Product Manager, Electrolytic Capacitors at BCcomponents. “The 197 series has been developed specifically to cater for customers who are looking for a high quality, cost-effective solution.”

The 197 PGP-SI capacitance range is 56 to 1800 μF, and its voltage range is 160 to 450 Volts, depending on case size. The category temperature range is −40 °C to +85 °C and the product's load life and useful life at 85 °C is 2000 hours, while its useful life at 40 °C is 25000 hours.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword