Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

New P-Channel ChipFETs Are First in Lead-Less Package with ESD Protection:New Power MOSFETs Aimed At Portable Designs with Plug-In Accessories


ChipFET

Products mentioned:

Si5461EDC
Si5463EDC
Si5465EDC
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

SANTA CLARA, CALIFORNIA - August 10, 2001 - Siliconix incorporated (NASDAQ:SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE:VSH) today announced the release of the first ESD-protected devices inits lead-less ChipFET® power MOSFET series. The new p-channel devices, which occupy a footprint measuring 3.05 by 1.80 mm, provide an extra measure of protection when used to switch power in systems with attachable/detachable accessories such as SIM cards, Blue tooth adapters, IrDA adapters, MP3 adapters, and cable connections to other portable equipment.

Designed to minimize conduction losses, the new ChipFETs additionally feature low on-resistance. For the three devices released today, rDS(on) at a 4.5-V gate drive is respectively 45 mΩ and 62 mΩ for the 20-V Si5461EDC and Si5463EDC, and just 37 mW for the 12-V Si5465EDC. All three devicesare also rated for operation at 2.5 V and 1.8 V. Maximum current handling ranges from 5.1 A to 7.0 A depending on gate-source voltage.

Typical applications for the new ChipFETs will include load switching, battery charger switching, and power amplifier switching in cell phones, PDAs, and other portable devices. In addition to giving designers more flexibility in how and where power circuitry is laid out, their 5000-VESD protection will help to increase manufacturing yields, since fewer devices will be affected by handling during the production process.

Lead-less Vishay Siliconix ChipFETs occupy approximately half the board area required by a leaded TSOP-6, allowing designers to shrink the power management circuitry for cell phones and notebook computers into about half the space previously needed. By eliminating the leads found in conventional MOSFET packages, ChipFETs allow designers to reclaim board space that would otherwise be wasted and thus to add new features or capabilities within a smaller area. And since maximum ChipFET thermal resistance is just 20°C/W, compared to 35°C/W for the TSOP-6, designers can handle more power, or build a cooler-running circuit, in addition to saving space.

Samples and production quantities of the Si5461EDC, Si5463EDC, and Si5465EDCare available now, with lead times of six to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

ChipFET is a trademark of Siliconix incorporated.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword