|
For more information: New Low-Profile, High-Current Inductors Enhance Space and Power Savings in DC/DC Converter ApplicationsSurface-Mount Vishay Dale Devices Improve Battery Performance, Help Reduce Size of Portable and Handheld Electronic Devices
MALVERN, PENNSYLVANIA - October 5, 2001 - Two new series of high-current inductors that combine low losses at frequencies up to 5 MHz, low DCR values, and a height profile that is 30% lower than in conventional solutions were announced today by Vishay Intertechnology, Inc. (NYSE: VSH). Designed for dc-to-dc converter and energy storage applications, the new Vishay Dale devices will be used to replace taller, larger, and/or lower-performing inductors, thus enabling lighter, thinner mobile and desktop computers, servers, cell phones, digital cameras, global positioning systems, and other handheld electronic products. New Vishay Dale IHLP-2525CZ-01 inductors measure 0.25 in. (6.47 mm) by 0.27 in. (6.68 mm), with a height profile of just 0.118 in. (3.0 mm). Dimensions for new IHLP-5050CE-01 devices are 0.508 in. (12.9 mm) by 0.520 in. (13.2 mm), with a height profile of 0.138 in. (3.5 mm). Standard inductance values in the IHLP-2525CZ-01 series range from 0.10 μH to 4.7 μH, and maximum DCR ranges from 1.7 milliohms to 40 milliohms at 100 kHz, depending on inductance. Maximum current handling ranges from 3.9 A to 22 A. The IHLP-5050CE-01 features a standard inductance range of 0.47 μH to 5.6 μH, maximum DCR values from 2 milliohms to 18 milliohms at 100 kHz, and current ratings from 6.5 A to 18 A. Alternative designs in the IHLP family have inductance ranges from 0.025 μH to 15μH with current ratings up to 48 A. Inductance tolerance for both devices is ±20%. At full rated current, each device has an inductance drop of less than 10%. Both inductor series are now available using an entirely lead-free construction. Samples and production quantities are available now. Lead time for production quantities is six to eight weeks.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |