Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

New Solid Tantalum Chip Capacitors Provide Industry's Highest Available Capacitance Ratings in Low-Profile Case

High Capacitance, Low ESR Values, and Low Profile Combine to Enable Lighter and Thinner Portable Handheld Appliances


For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

MALVERN, PENNSYLVANIA - February 15, 2002 - Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two additions to the 592Dfamily of solid tantalum chip capacitors, which nowprovides the industry's highest available capacitance in a low-profile case.

Designed for noise suppression and capacitive decoupling applications in slim-line products including wireless PCMCIA cards and cell phones, the new 592D devices in low-profile "X" and "Y" cases feature exceptionally low equivalent series resistance (ESR) values, reducing power consumption while enabling thinner and lighter end products.

The new Vishay Sprague 592D devices, part of the TANTAMOUNT® product line, feature high capacitance ratings ranging from 1000 μF to 2200 μF, with standard tolerances of ±10% and ±20%. The capacitors' ultra-low maximum ESR values range from 0.035 Ω to 0.04 mΩ at +25°C and 100 kHz. The X and Y cases feature dimensions of 0.570 in. [14.5 mm] by 0.290 in. [7.37 mm] with maximum height profiles of just 0.078 in. [2.0 mm] and 0.098 in. [2.5 mm], respectively.

Working voltage options range from 4 WVDC to 6.3 WVDC. Maximum current leakage ranges from 60 μA to 95 μA, and the maximum dissipation factor ranges from 16% to 25% at +25°C and 120 Hz. The 592D capacitors feature an operating temperature of −55°C to +85°C, up to +125°C with voltage derating. The new devices are conformal coated and feature two standard 100% tin terminations.

The capacitors' low height profiles enable the design of more compact endproducts for increased convenience and portability. In some applicationsthese high-capacitance devices from the 592Dfamily may be used to replace several capacitors with lower ratings.

Samples and production quantities of the 592D X- and Y-size capacitors are available now in tape-and-reel packaging, with lead times of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TANTAMOUNT is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword