Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Media contact -  Peter Frey, Vishay Semiconductor GmbH
Phone:  +49 7131 67 2376 
Fax:  +49 7131 67 2423 
E-mail:  peter.frey@vishay.com

Second-Generation Dual MOSMICs® Bring Superior AGC, Cross-Modulation, and Dynamic Performance to UHF and VHF Tuner Applications


Analog Switches
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Media contact -  Peter Frey, Vishay Semiconductor GmbH
Phone:  +49 7131 67 2376 
Fax:  +49 7131 67 2423 
E-mail:  peter.frey@vishay.com

MALVERN, PENNSYLVANIA - April 10, 2002 - Vishay Intertechnology, Inc. (NYSE: VSH) has launched its second-generation family of dual MOSMICs® - MOS monolithic integrated circuits that combine two automatic gain controlled (AGC) amplifiers on a single chip.

Rated for 5-V operation, the new "X" series dual MOSMICs (previously marketed under the Vishay Telefunken name) provide superior automatic gain control, cross-modulation behavior, and dynamic performance when used as low-noise input stages for UHF and VHF tuners in television sets and set-top boxes. The new devices serve as drop-in- and function-compatible upgrades to Vishay's previous-generation MOSMICs, allowing designers to upgrade system performance at no additional cost.

The dual MOSMICs released today offer a choice of typical transadmittance specifications: 24 ms for the TSDF52424X/XR and TSDF02424X/XR, 30 ms for the TSDF53030X/XR and TSDF03030X/XR, and 40 ms for the TSDF54040X/XR and TSDF04040X/XR. All six devices feature a low noise figure of just 1 dB at 200 MHz, and enhanced typical cross modulation of 105 dBV at a 40-dB AGC. The X series dual MOSMICs also feature reduced input capacitance as low as 1.7 pF, an improvement of nearly 20% over previous-generation devices.

Integrated gate protection diodes and resistors and an on-chip biasing network allow designers to eliminate a number of external passive components. The combination of two AGC amplifiers on a single chip allows designers to combine two bands on a single device, eliminating the need for separate ICs to handle VHF and UHF bandwidths. All six devices are packaged in a compact SOT363 surface-mount package that allows reverse pinning and saves space with dimensions of just 2.05 mm by 1.25 mm.

With their improved performance, the X series dual MOSMICs represent a new industry standard for high-volume, cost-effective applications. A general type designation enables designers to identify the most suitable upgrade device for a given application. The TSDF52424X/XR, TSDF53030X/XR, TSDF54040X/XR, TSDF02424X/XR, TSDF03030X/XR, and TSDF04040X/XR are rated for a 5-V supply voltage and can be used to replace previous-generation MOSMICs with equivalent transadmittance specifications.

Samples and production quantities of the new dual MOSMICs are available now, with lead times of four to eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword