Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

This BCcomponents product press release (excluding the datasheet links and paragraph on Vishay) originally appeared on the former BCcomponents Web site.

Glass coated SMD thermistors with nickel barrier termination


Thermistor

Products mentioned:

2322 615 3x
2322 615 5x
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

December 11, 2002 — Delivering high sensitivity and high accuracy over a wide temperature range, the latest thermistors from BCcomponents (BCc) are fully covered with glass for environmental protection and feature nickel barrier contacts for improved soldering characteristics.

BCc’s surface mount series 2322 615 3x and 2322 615 5x negative temperature coefficient (NTC) chip thermistors are ideal for temperature compensation, sensing, and protection circuits in applications such as battery chargers, switch mode power supplies and automotive systems. The devices will also suit designs for temperature regulation of optoelectronic components including laser diodes and CCDs.

Available in 0603 and 0805 surface mount packages, the 2322 615 3x (0603) and 2322 615 5x (0805) NTC thermistors feature R25 values (resistance at 25 °C) from 2.2kΩ to 100kΩ. Standard R25 tolerance options are ±2%, ±3%, ±5% and ±10% and a ±1 option is available on request. Calibration constant tolerance from 25 °C to 85 °C (ß25/85) is just ±1%, ensuring high sensitivity and high accuracy across a wide temperature range.

Available in paper tape-and-reel format, the 2322 615 3x and 2322 615 5x thermistors are fully compatible with high-volume, automated manufacturing processes including wave soldering and reflow soldering in accordance with CECC00802. A tin plated nickel termination provides better wettability and improved reliability against leaching compared with conventional silver/palladium solutions. In addition, problems associated with silver migration are eliminated. Operating temperature for the devices is specified as −40 °C to 150 °C, while maximum power dissipation at 25 °C is 125 mW.

BCcomponents’ recent investment in new, fully automated production equipment has enabled the company to now process several hundreds of millions of thermistors.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword