|
For more information: Vishay's New 500-mA LDO Regulator Combines 150-mV Dropout Voltage and 1-μA Ground Current in Ultra-Compact MLP33 PowerPAK™ Package
SANTA CLARA, CALIFORNIA - December 20, 2002 - Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology (NYSE: VSH), has announced the launch of the Si9185, a 500-mA CMOS low dropout (LDO) regulator that features very low dropout and ground current in an exceptionally compact, thermally enhanced MLP33 PowerPAK™ package. With low dropout of just 150 mV at 500 mA, and a tiny 3-mm by 3-mm footprint - 70% smaller than the industry-standard SO-8 package - the new Si9185 is designed to prolong battery life in compact, portable electronics including notebook computers, PDAs, digital cameras, and smart phones; or in SMPS. Vishay's Si9185 LDO is specified for input voltages from 2 V to 6 V and is available in 10 fixed voltage options ranging from 1.2 V to 5.0 V, as well as in adjustable output voltage options. The device features noise output of 100 μV(rms) with a noise bypass capacitor, 1.5% output voltage accuracy, 1.1-W power dissipation, and a maximum shutdown current of 1 μA. If a capacitor is connected to the device's delay pin, the Si9185's out-of-regulation error flag output pin will generate a delayed power-on-reset signal. Integrated short-circuit and thermal protection ensure reliable operation over the regulator's operating temperature range of -40°C to +85°C. The Si9185 serves as a highly cost-effective and compact solution that offers line/load transient response and ripple rejection superior to that of bipolar or BiCMOS LDO regulators. The new device also is compatible with low-ESR ceramic capacitors or tantalum capacitors, providing designers with flexibility in choosing magnetic components. Samples and production quantities of the Si9185 are available now with lead times of eight weeks for larger orders.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. PowerPAK is a registered trademark of Siliconix incorporated. |