VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2003 Releases:Military Established Reliability Foil Resistors
For more information:
Media contact: Andrew Post, Sr. Manager, Global Communications
phone 1.610.251.5287  fax 1.610.889.9429  e-mail andrew.post@vishay.com
 

RNC90Z Military Established Reliability Foil Resistors Offer Resistance Range Extension up to 121 KΩ With Low TCR of ±2 ppm/°C

MALVERN, PENNSYLVANIA — March 31, 2003 — Vishay Intertechnology, Inc. (VSH: NYSE) today announced that it has extended the resistance range of the RNC90Z family of military established reliability foil resistors up to 121 KΩ with a very low TCR of 2.0 ppm/°C, a value 2.5 times better than provided by the RNC90Y.

As "R" level established reliability resistors, RNC90Z resistors are military-qualified to MIL-PRF-55182/9 with characteristic "Z" limits. The new resistors are designed for use in military and aerospace applications and in other applications requiring established reliability and precision performance.

The Vishay Foil Resistors RNC90Z resistor series, which is based on Vishay's technologically advanced, ultra-precision, low-TCR "Z" Bulk Metal® foil, serves as a direct replacement for the RNC90Y series, which has long been the benchmark for discrete established reliability resistors. The devices released today offer a similarly priced alternative to the RNC90Y, now with a broad resistance range of 100 Ω to 121 KΩ, in addition to standard resistance tolerances from ±1.0% down to ±0.01% and very low TCR values over an extended temperature range of -55°C to +175°C.

The devices' power rating is 0.6 W at +70°C and 0.3 W at +125°C, with a maximum working voltage of 300 V. Each resistor measures 0.105 in. by 0.300 in. (2.67 mm by 7.62 mm), with a height of 0.326 in. (8.28 mm), and typically weighs 0.6 grams.

Samples and production quantities of the extended-range RNC90Z resistors are available now. Lead time for production quantities is approximately 12 weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal is a registered trademark of Vishay Intertechnology, Inc.

 
foil resistors
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account