VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2003 Releases:New Vishay Model 21P Molded Plastic Dial
For more information:
Media contact: Andrew Post, Sr. Manager, Global Communications
phone 1.610.251.5287  fax 1.610.889.9429  e-mail andrew.post@vishay.com
 

New Vishay Model 21P Molded Plastic Dial Features Excellent Readability and Precision Feel in Turn Counting for Rotary Potentiometers

MALVERN, PENNSYLVANIA - April 9, 2003 - A new plastic, 11-turn dial with a 46-mm [1-13/16-in.] diameter was announced today by Vishay Intertechnology, Inc. (NYSE: VSH). The new Vishay Spectrol Model 21P is designed to serve as a counting turn dial for industrial control applications in which there is a need to read the number of turns of a transducer shaft.

The Model 21P features a round Vernier scale on its graduated dial, providing excellent readability and precision feel, as well as high accuracy and a locking brake to keep the reading set. To eliminate guesswork, a mechanism on the dial sounds an alert to the user when a full cycle has been completed. The device’s window indicates the completed number of turns of the drive sleeve, while the graduated circular dial indicates the percent of the partial turn of the drive sleeve. Readouts increase with clockwise motion and decrease with counter-clockwise motion. The Model 21P is capable of displaying readings of up to 1099 turns.

The dial may be mounted directly to the transducer shaft with an Allen key included - along with mounting instructions - under the same part number. A 6﷓mm adapter also is available in the dial package. With a clear, metallized (aluminum) finish over a plastic ABS mold, the new dial offers a high-quality, cost-efficient alternative to chrome metal dials. The Model 21P weighs just 13 grams and is suitable for use with all rotary transducers.

Samples and production quantities of the Vishay Spectrol Model 21P are available now, with lead times of four to six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Dial
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account