VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2003 Releases:New CSM Ultra-Precision Resistors
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-discrete/sales
 

Vishay's New CSM Ultra-Precision, 2-mΩ, Surface-Mount, Current-Sensing Resistors Provide TCR Values Down to ±15 ppm/°C and Superior Stability in Compact 2512 and 3637 Sizes

MALVERN, PENNSYLVANIA - May 15, 2003 - Vishay Intertechnology, Inc. (VSH: NYSE) today announced a new series of ultra-precision, 2-m Ω, surface-mount, current-sensing resistors featuring a four-terminal (Kelvin) design and TCR values as low as ±15 ppm/°C for uniquely high stability and performance in voltage division and precision current-sensing applications.

Intended for switching linear power supplies, power amplifiers, and measurement instrumentation, the compact CSM2512 and CSM3637 resistors from Vishay Foil Resistors feature an all-welded construction made up of a Bulk Metal® resistive element with 60/40 tin/lead-plated copper terminations. Vishay's Bulk Metal technology enables the new resistors to provide superior TCR performance over larger, competing devices, as well as excellent long-term stability and ultra-precision tolerances down to ±0.1%.

The CSM2512 features a 1-W power rating over its entire resistance range from 3 mW to 200 mΩ, while the CSM3637 is rated for 3 W from 2 mΩ to 10 mΩ and for 2 W from >10 mΩ up to 200 mΩ. In addition to low ohmic values, the CSM2512 and CSM3637 offer compact dimensions of just 0.25 in. by 0.125 in. [6.35 mm by 3.175 mm] and 0.360 in. by 0.370 in. [9.14 mm by 9.4 mm], respectively, with a height profile of 0.025 in. [0.635 mm].

Both new devices are specified for an operating temperature range of -55°C to +125°C. Depending on the specific requirements of their applications, designers may choose from tolerance options of ±0.1%, ±0.25%, ±0.5%, and ±1.0%.

Available in waffle-pack or tape-and-reel packaging, samples and production quantities of the CSM series resistors are available now. Lead time for production quantities is approximately 12 weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal is a registered trademark of Vishay Intertechnology, Inc.

 
CSM Ultra-Precision Resistors
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account