|
For more information: Vishay Extends IHLP Family of Low-Profile, Surface-Mount Inductors With New Devices Rated for Saturation Currents up to 120 A and Typical DCR Values as Low as 0.47 mΩ
MALVERN, PENNSYLVANIA - May 23, 2003 - Vishay Intertechnology, Inc. (NYSE: VSH) today announced the IHLP-5050FD-01 series, a new low-profile, high-current inductor with typical DCR values as low as 0.47 m Ω and low losses at frequencies up to 5 MHz. This latest addition to the patented Vishay Dale IHLP family of compact, surface-mount inductors is designed to provide a higher-performing, power- and space-saving solution for dc-to-dc converter and energy storage applications in end products including computers, servers, telecom, and automotive electronics. Devices in the IHLP-5050FD-01 series are offered in a surface-mount package measuring just 0.508 in. (12.9 mm) by 0.520 in. (13.2 mm), with a height profile of 0.256 in. (6.5 mm). The inductor 's high saturation current ranges from 30 A to 120 A, and its maximum DCR values range from 0.50 m Ω to 11.2 m Ω. Standard inductance values range from 0.10 μ H to 4.7 μ H, with a tolerance of ± 20%. At full rated current, the IHLP devices feature an inductance drop of less than 20% - a lower inductance roll-off than is provided by ferrite materials. IHLP-5050FD-01 inductors feature a self-shielded package and meet military specifications for resistance to thermal shock, moisture, mechanical shock, and vibration. Samples and production quantities are available now. Lead time for production quantities is six weeks.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |