Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

New Heavy-Duty, Metallized-Film Power Capacitors Offer Current Ratings up to 150 A and Low Self-Inductance in Compact, Easy-Mounting Radial Design


Capacitors

Products mentioned:

HDMKP
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

MALVERN, PENNSYLVANIA — June 8, 2003 — A new series of heavy-duty, metallized-film power capacitors with current ratings as high as 150 A and very low self-inductance was announced today by Vishay Intertechnology, Inc. (NYSE: VSH).

The new Vishay ESTA HDMKP series devices serve as low-cost capacitor solutions for dc and ac filtering and for dc linking in uninterruptible power supplies and in power converters for traction and industrial drives.

In addition to exceptionally low inductance and high current ratings, the new HDMKP capacitors offer extremely low losses at high frequencies, low ESR, and high reliability and life expectancy in a compact design.

Inductance for the new capacitor series is less than 50 nH, and the devices' dissipation factor is less than 8 x 10-4 at a frequency of 1 kHz. An advanced metallized film on the capacitors' polypropylene dielectric enables the devices to offer a high RMS current rating, while series resistance of less than 5 mΩ allows them to reduce ohmic losses.

HDMKP capacitors are available in six standard voltages from 900 V to 2700 V (dc) and from 220 V to 660 V (ac), with voltages up to 4800 V (dc) available on request. Capacitance values range from 40 μF to 1100 μF, with a capacitance tolerance of ±5%. Non-standard capacitance values also are available to designers on request.

Heavy-duty resistance to shock and vibration, as well as a reliability rating of 300 FIT, contribute to the devices' lifetime expectancy of 100,000 hours at +60°C at rated voltages. Devices in the HDMKP series are specified for an operating temperature of -40°C to +70°C at full rated voltage, or up to +100°C at half of the rated voltage, and meet IEC 61071-1, EN 61071, IEC 68-2, and IEC 61881 standards. Terminal-to-terminal test voltage is 1.5 times the rated dc voltage for 10 seconds.

Capacitor height options range from 105 mm to 260 mm, with a standard diameter of 84.4 mm. The devices' non-polar dielectric is housed in an aluminum/lathene casing with a dry resin filling. An integrated M12 stud at the capacitor base enables easy mounting.

Samples and production quantities of the new HDMKP series capacitors are available now, with lead times of eight weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###
Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword