![]() |
|
||||||
|
|
|
For more information:
Media contact: e-mail andrew.post@vishay.com Sales contact: http://www.vishay.com/resistors-networks/sales Vishay's New SMN Ultra-Precision Bulk Metal® Foil Resistor Network Offers Tracking TCR of 1 ppm/°C and Stability of 0.01% at 0.1 W in Eight-Pin, Surface-Mount PackageMALVERN, PENNSYLVANIA July 7, 2003 Vishay Intertechnology, Inc. (VSH: NYSE) today announced the release of the SMN series of four-resistor, surface-mount, ultra-precision Bulk Metal® Foil resistor networks, the industry's first devices to provide a low tracking TCR of 1 ppm/°C and high stability of 0.01% at 0.1 W in a small-outline, eight-pin, industry-standard JEDEC MS-012 package. Each SMN resistor network is made up of four independent Bulk Metal Foil resistors in a dual in-line, molded epoxy package measuring just 0.157 in. by 0.195 in. [3.99 mm by 4.93 mm] with a 0.068-in. [1.73-mm] height profile and a 50-mil lead pitch. This compact, integrated construction offers space savings and improved electrical performance over discrete resistors and matched sets, providing TCR absolute value of ±5 ppm/°C and TCR tracking value of ±1 ppm/°C. Eight resistance values between 100 Ω and 10,000 Ω allow the series to offer a broad range of resistance ratios from 1.0:1 to 100:1, with a tight resistance ratio tolerance of ±0.01% and absolute tolerance of ±0.02%. The power rating is 0.4 W for the entire package at 70°C, or 0.1 W per resistor. Resistance to thermal shock, shock, moisture, high-frequency vibration, and extreme temperatures contribute to long-term device stability, which surpasses that of competing products by a factor of 2. Low thermal EMF of 0.04 µV/°C and low current noise of 0.01 µV/V(RMS) at -40 dB serve to enhance device performance. These new resistor networks, which may be used independently or as divider pairs, are designed for use in precision instrumentation amplifiers, differential amplifier gain controls, matched references, and precision voltage dividers in automated test equipment and measurement instrumentation, as well as in precision weigh scales. Devices in the new SMN series from Vishay Foil Resistors feature solder-coated copper-alloy terminals and weigh just 0.08 g. Available in tube, waffle-pack, or tape-and-reel packaging, samples and production quantities of the SMN series resistor networks are available now. Lead time for production quantities is approximately 12 weeks. Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. ###
Bulk Metal is a registered trademark of Vishay Intertechnology, Inc. | ![]() | ||||
![]() |
|||||
| ||||||