VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2003 Releases:New DSM Ultra-Precision, Surface-Mount Foil Resistor Dividers
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-networks/sales
 

Vishay's New DSM Ultra-Precision, Surface-Mount Foil Resistor Dividers Provide Stability of 0.01% at 0.05 W, Tracking Values Down to 1 ppm/°C

MALVERN, PENNSYLVANIA —July 11, 2003 — Vishay Intertechnology, Inc. (VSH: NYSE) today announced the release of the DSM series of ultra-precision, surface-mount resistor dividers, which integrate a matched pair of Bulk Metal® Foil resistors featuring excellent stability and industry-leading TCR performance with absolute values of 5 ppm/°C and tracking values of 1 ppm/°C or better.

These new Vishay Foil Resistors dividers incorporate a two-resistor, three-terminal resistor network in a compact molded, epoxy package measuring 0.16 in. by 0.106 in. [4.0 mm by 2.7 mm]. The electrical performance of this integrated construction provides superior performance and improved use of space compared with discrete and matched-pair resistors. High stability of 0.01% at 0.05 W and 70°C over 2,000 hours also sets these dividers apart from competing devices.

The DSM series is intended for precision instrument amplifier applications, differential gain control, and precision voltage division applications in automated test equipment and measurement instrumentation, as well as in precision weigh scales and voltage dividers.

Resistance values of 100 Ω to 10 kΩ are available in a broad range of resistance ratios from 1:1 to 100:1, with a tight resistance-ratio tolerance as low as ±0.01%. Absolute tolerance is 0.02%. The DSM divider features a power rating of 0.1 W for the entire package at 70°C, or a rating of 0.05 W per resistor. The series' performance is enhanced by low thermal EMF of 0.1 µV/°C and low current noise of 0.01 µV/V(RMS) at -40dB.

DSM resistor dividers, which feature silver-coated copper-alloy terminals, weigh just 0.04 g and offer resistance to thermal shock, shock, moisture, high-frequency vibration, and extreme temperatures. They are specified for an operating temperature range of -65°C to +150°C.

Available in bulk-pack or tape-and-reel packaging, samples and production quantities of the DSM series resistors are available now.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Bulk Metal is a registered trademark of Vishay Intertechnology, Inc.

 
Foil Resistors
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account