VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2003 Releases:New Surface-Mount, Current-Sensing Transformers
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/transformers/sales
 

Vishay's New Surface-Mount, Current-Sensing Transformers Offer Versatile, Lead-Free Construction and Five Standard Turns Ratios From 30 to 125

MALVERN, PENNSYLVANIA — July 25, 2003 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the new LPE-3325-CST series of surface-mount, current-sensing transformers featuring five standard turns ratios from 30 to 125 in a lead (Pb)-free construction.

Designed to provide optimal performance at frequencies of 100 kHz and greater, the new LPE-3325-CST is intended for switching power supplies, ac current detection, and output supplies for control circuitry in household appliances and medical and office equipment.

Available with turns ratios of 30, 40, 50, 70, and 125, the transformer released today by Vishay Dale features secondary inductance ranging from 180 µH to 3000 µH at 100 kHz and 0.1 V and a maximum secondary resistance range of 1.00 Ω to 7.70 Ω. All five configurations are rated for 6 A.

Each transformer measures 0.265 in. by 0.323 in. [6.73 mm by 8.20 mm], with a 0.205-in. [5.21-mm] height profile. Custom configurations are available on request. The new devices are specified for an operating temperature range of -40°C to +130°C and are compatible with surface-mount process temperatures.

Samples and production quantities of LPE-3325-CST current-sensing transformers are available now. Lead-time for production quantities is 8 to 10 weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Transformers
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account