|
For more information: New 150-V High-Barrier-Height Schottky Rectifiers Offer Low Forward Voltage Drop, Low Leakage, and Maximum Junction Temperature of 175°C
MALVERN, PENNSYLVANIA — September 5, 2003 — A new series of 150-V high-barrier-height Schottky rectifiers offering a low forward voltage drop and leakage current under high-temperature operating conditions was announced today by Vishay Intertechnology, Inc. (NYSE: VSH). Intended for use in high-frequency inverters, freewheeling, switch-mode power supplies (SMPS), and polarity protection applications in power supplies and adapters, the Vishay Semiconductors MBR Series 150-V H-type dual-rectifier devices provide industry-leading specifications not only with respect to forward voltage and high reverse energy, but also for maximum average forward rectified current – 10 A in the TO-220 package outline. Built on a proprietary Schottky barrier technology, the new devices offer a typical forward voltage drop as low as 0.65 V, typical leakage current as low as 0.15 mA at 125°C, and high maximum operating junction temperature of 175°C. A reverse surge capability of 25 kV ESD and inductive reverse avalanche energy ratings up to 20 mJ enhance reliability. Forward voltage options of 10 A, 20 A, and 30 A are available for devices in TO-220, ITO-220, and TO-262 package outlines. These specifications represent an order of magnitude improvement over previous-generation Schottky rectifiers, with a reduction of leakage current by as much as half and a four-fold improvement in avalanche energy. The new devices are the latest in the Vishay "H" series, which takes advantage of a phenomenon known as conductivity modulation to achieve low leakage current and a high operating temperature in a Schottky rectifier without increasing barrier height and thus worsening voltage drop performance. The result is a device that combines low leakage current, a high operating temperature, and low forward voltage drops to allow efficient operation with low losses even during high-frequency and high-temperature operation. H-type series devices' metal-silicon junction is built using a proprietary sputtering process that guarantees a well-controlled barrier height. The resulting majority carrier conduction causes a forward voltage drop that is lower than a p-n junction rectifier, with negligible reverse recovery time. An ion-implanted guardring technology provides excellent reverse energy capability, thereby ensuring overvoltage protection. Samples and production quantities of the new H-type high-barrier-height Schottky rectifiers are available now, with lead times of four weeks for larger orders. Product data sheets are available for:
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. |