Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

Vishay Adds to 592D Family of Low-Profile Tantalum Capacitors: New Devices Offer 2200 μF Capacitance in 2 mm Case Height, 3300 μF in 2.5 mm Case Height

Compact, high-capacitance devices enable design of lighter, thinner wireless products


TANTAMOUNT
For more information:
Media contact -  Andrew Post, Sr. Manager, Global Communications
Phone:  1.610.251.5287 
Fax:  1.610.889.9429 
E-mail:  andrew.post@vishay.com

Sales contact: 

MALVERN, PENNSYLVANIA — October 31, 2003 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of two new devices in the 592D family of solid tantalum chip capacitors, which provides the highest available capacitance values for low profile tantalum capacitors.

Part of the Vishay Sprague TANTAMOUNT® product line, these new capacitors are designed for low-profile applications, such as wireless GPRS PCMCIA modem cards and cell phones, requiring very high capacitance.

The devices' low ESR values help to reduce power consumption, while their uniquely compact case size enables the design of lighter, smaller, more portable end products. In some applications, these high-capacitance devices may be used to replace several capacitors with lower ratings, allowing designers to conserve board real estate and decrease component count.

The 592D capacitors released today are available in "X" and "Y" cases with dimensions of 0.570 in. by 0.290 in. [14.5 mm by 7.37 mm] and height profiles of 0.079 in. [2.0 mm] and 0.098 in. [2.5 mm], respectively. The 592D228X_6R3X2_ in the X case features capacitance of 2200 μF and a maximum current leakage of 139 μA. In the Y case size, the 592D338X_6R3Y2_ offers a capacitance value of 3300 μF and maximum current leakage of 208 μA.

At 6.3 WVDC both devices offer a maximum dissipation factor of 35%, very low ESR of 0.055 Ω, and ripple of 1.80 A during operation at +25 °C and 100 kHz. Capacitance tolerances of ±10% and ±20% are standard.

Tantalum capacitors in the 592D family are conformal coated, feature two 100% tin terminations, and are case-code compatible with EIA 535BAAC and CECC 30801 molded chips. The devices are specified for an operating temperature range of -55 °C to +85 °C.

Samples and production quantities of the new 592D228X_6R3X2_ and 592D338X_6R3Y2_ capacitors are available now in tape-and-reel packaging, with lead times of seven weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TANTAMOUNT is a registered trademark of Vishay Intertechnology, Inc.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword