|
For more information: Siliconix's 7-nC P-Channel MOSFET Enables Design of Simplified, High-Efficiency Synchronous Buck DC/DC Converters for Handheld Electronics
SANTA CLARA, CALIFORNIA — November 3, 2003 — In a breakthrough that will help designers reduce the size of dc-to-dc converters in the smallest handheld electronic systems, Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH) today announced the industry's first p-channel power MOSFET optimized for use in synchronous buck converters. Used on the synchronous buck high-side, a p-channel MOSFET can be turned on with a gate drive that is lower than the battery voltage. This eliminates the need for extra bootstrap circuitry, simplifying and shrinking dc-to-dc converter designs. The new Vishay Siliconix Si3867DV takes this space-saving p-channel benefit a step further by optimizing the device for low switching losses, ensuring efficient operation at high frequencies. Combining on-resistance of 0.051 ohms with an extraordinarily low typical gate charge of 7 nC, the Si3867DV delivers an on-resistance-times-gate-charge figure of merit (FOM) of 0.36, which is 28% better than the next best competing p-channel MOSFET on the market. In addition to this low FOM value, the Si3867DV has been optimized with a low Qgd/Qgs ratio of 0.7 to eliminate secondary turn-on effects. Packaged in the LITTLE FOOT® TSOP-6, the -20-V Si3867DV will be used for low-current buck and inverter dc-to-dc converters in end products including cell phones, SIP cards, PDAs, digital still and video cameras, and hard disk drives. Additional applications include notebook computer synchronous buck converters for auxiliary voltages and asynchronous buck converters for smart battery packs. This is the first in a planned series of PWM-optimized p-channel MOSFETs. Future entries in the series will include devices with -12-V and -30-V breakdown voltages and optional on-board Schottky diode in a range of surface-mount LITTLE FOOT and PowerPAK® packages. Samples and production quantities of the Si3867DV are available now, with lead times of 8 to 10 weeks for larger orders. Siliconix is a leading manufacturer of power MOSFETs, power ICs, analog switches, and multiplexers for computers, cell phones, fixed communications networks, automobiles, and other consumer and industrial electronic systems. With 2002 worldwide sales of $372.9 million, the Company's facilities include a Class 1 wafer fab dedicated to the manufacture of power products in Santa Clara, California, and an affiliated Class 1 wafer fab located in Itzehoe, Germany. The Company's products are also fabricated by subcontractors in Japan, Germany, China, and Taiwan. Assembly and test facilities include a company-owned facility in Taiwan, a joint venture in Shanghai, China, and subcontractors in the Philippines, China, Taiwan, Israel, and the United States.
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com. LITTLE FOOT and PowerPAK are registered trademarks of Siliconix incorporated. |