VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:Sealed Weldable Strain Gages
For more information:
Media contact: e-mail marti.spalding@measurementsgroup.com
Sales contact: http://www.vishay.com/brands/measurements_group/sales
 

New Vishay Micro-Measurements Sealed Weldable Strain Gages Provide Easy Installation and Withstand Water Pressure to 500 psi, Temperatures up to +180 °F

MALVERN, PENNSYLVANIA — February 10, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) has released a new series of Sealed Weldable Strain Gages designed to provide easy installation and reliable performance for test and measurement applications, such as stress analysis testing, in a variety of demanding installations and environments.

The new strain gages from Vishay Micro-Measurements are specially designed to accommodate spot welding to structures and components in circumstances that preclude clamping and curing an adhesively bonded gage installation, or when high temperatures prevent the use of an elevated-temperature-curing adhesive. Each gage is pre-bonded with a high-performance adhesive to a thin 0.005 in. [0.127 mm] stainless steel carrier. To increase reliability and reduce the time and labor required for installation, each gage is sealed in-factory, fully encapsulated with a protective coat that provides resistance to moisture.

Three leadwire configurations are available to provide the best fit for a given application, environment, and/or installation. Gages in the R leadwire series are designed for long-term, outdoor use in applications such as railroad and civil structures, where they may be exposed to oil and water splash or short-term submersion. These gages feature a metal carrier processed to give good first-cycle data, excellent fatigue resistance, and a high strain range.

The T leadwire series of Sealed Weldable Strain Gages is typically used in larger civil structures including bridges, dams, and buildings, or in applications with exposures of up to a year in sea water. These gages are designed to withstand exposure to water pressures of up to 500 psi, as well as short-term (up to 14 days) immersion in crude oil. A flexible, stainless steel tube provides wire routing from the strain gage to a cable transition, thereby facilitating fine positioning of the sensor and providing strain relief.

Gages in the L leadwire series offer performance comparable to that of gages in the T leadwire series and - without an integrated cable transition - a more compact configuration that enables their use in applications with greater space constraints. These gages are suited for applications with smaller strains, but anchoring the leadwire during installation can provide for strain relief.

All three gage configurations feature nominal resistance of 350 Ω, a nominal gage factor of 2.0, a gage length of 0.125 in., and a shielded vinyl leadwire. Both axial and shear grid geometries are available. Vishay's Sealed Weldable Strain Gages have a ±5000 microinch/in. strain range and a normal operating temperature range of +32 °F [0 °C] to +180 °F [+83 °C]. Gages in this series may be installed on surfaces with a radius of curvature of 3.0 in. [76 mm] or greater.

Vishay Micro-Measurements is a division of Vishay Measurements Group. Vishay Measurements Group develops, manufacturers, and markets a broad range of sensors for a wide variety of test and measurement applications. These include electrical resistance strain gages for both stress analysis testing and transducer manufacturing applications, instrumentation, and hybrid strain gage assemblies under the Vishay Micro-Measurements and BLH brands, and transducers for OEM applications and certified load cells for electronic scales and other weighing applications under the Vishay Nobel, Sensortronics, Tedea-Huntleigh, BLH and Celtron brands. Vishay Measurements Group is part of Vishay Intertechnology.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Sealed Weldable Strain Gages
 

Products mentioned:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account