Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay’s New Zener Diode Series Offers High Reliability and Voltage Range From 2.4 V to 15 V in Tiny SOD 523 Package

New Diodes Provide Space-Saving Solution for Portable Electronic Devices


Diodes

Products mentioned:

BZX584Cxx-02
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

MALVERN, PENNSYLVANIA — March 19, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new Zener diode series in the ultra-small SOD 523 (SC79) plastic package, which features very small dimensions of 1.2 mm by 0.8 mm with a 0.6 mm height profile.

The new BZX584Cxx 02 series Zener diode from Vishay Semiconductors, rated for a voltage range of 2.4 V to 15 V, is designed specifically for space-sensitive voltage-regulation applications in portable communications and computing devices including cellular and cordless phones, Bluetooth products, digital cameras, MP3 players, notebook computers, and PDAs.

These diodes feature a notably high power dissipation value of 200 mW given their extremely compact package size. An innovative die and lead-frame technology provides for a low thermal resistance of just 600 K/W.

Each of the new diodes weighs just 1.5 mg and is available in tape and reel packaging. Samples and production quantities of the new Zener diode series in the SOD 523 package are available now, with lead times of eight to ten weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword