Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Siliconix Targets Automotive 12-V Boardnet With New P-Channel −40-V and −60-V TrenchFET® Power MOSFETs

Up to 90% Lower On-Resistance Than Industry’s Next-Best Devices


For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

SANTA CLARA, CALIFORNIA — March 29, 2004 — Automotive 12-V boardnet high-side switches and electric motor drives are the target applications for a record-setting family of p-channel MOSFETs announced today by Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH).

The new −40-V and −60-V devices are the first with these breakdown voltage ratings to be built using Vishay’s advanced p-channel technology, which reduces MOSFET on-resistance to record-low levels. Maximum rDS(on) ratings range from 15 mΩ down to 4.2.mΩ for the six devices released today.

Because p-channel MOSFETs require no additional high-side driver circuitry for turn-on, these new −40-V and −60-V TrenchFETs will help designers to reduce component count and improve reliability in automotive and industrial systems compared with n-channel solutions.

When used to replace previous-generation p-channel devices, the new TrenchFETs give designers the opportunity to lower system power consumption as well. Compared with the next-best p-channel MOSFETs on the market with the same voltage ratings and package outlines, conduction losses for the new devices are reduced by up to 90%.

Package options for the −40-V devices are the standard DPAK (SUD50P04-09L), the thermally enhanced D2PAK (SUM110P04-04L), and the lead-less, 1.07 mm-high PowerPAK® SO-8 (Si7463DP). The −60-V TrenchFETs also are offered in the DPAK (SUD50P06-15L), the thermally enhanced D2PAK (SUM110P06-07L), and PowerPAK SO-8 (Si7461DP). The DPAK and D2PAK devices are rated for a maximum junction temperature of 175 °C, while the PowerPAK SO-8 TrenchFETs are rated for up to 150 °C.

Summary of Device Specifications

Device

VDS (V)

R(DS)on at 10 V (mΩ)

Max ID (A)

Package

SUM110P04-04L

−40

4.2

−110

D2PAK

Si7463DP

−40

9.2

−18.6

PowerPAK SO-8

SUD50P04-09L

−40

9.4

−50

DPAK

SUM110P06-07L

−60

6.9

−110

D2PAK

Si7461DP

−60

14.5

−14.4

PowerPAK SO-8

SUD50P06-15L

−60

15

−50

DPAK

Samples and production quantities of the new p-channel TrenchFET power MOSFETS are available now with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword