VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:New PR Series High-Precision Thin Film Resistor Arrays
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistor-networks/thin-film/resistor-arrays/
 

Vishay's New PR Series High-Precision Thin Film Resistor Arrays Offer Ultra-Low 0.01% Ratio Tolerance in Low-Profile, 0.4 mm-High Packages

MALVERN, PENNSYLVANIA — July 16, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the PR series high-precision thin film resistor arrays in compact 1206, 0805, and 0603 case sizes with a low profile of just 0.4 mm. Vishay is the only manufacturer to offer 0.01% ratio tolerance as a standard product feature in such low-profile arrays.

Matched resistor networks in the PR series include from two to eight resistors and are precision-matched to 0.01% ratio tolerance - as opposed to a ratio tolerance of 0.05% in competing devices. The new resistor arrays serve as compact replacements for larger-package devices - those utilizing wirewound or hermetic packaging - in instrumentation amplifiers, precision voltage dividers, bridge network circuitry, and all other products requiring a matched pair or set of resistor elements.

The new devices feature a highly stable TAMELOX® (passivated nichrome) resistive layer. PR series resistor arrays are specified for anabsolute TCR (temperature coefficient ratio) of 10 ppm/°C and TCR tracking of 2 ppm/°C - or down to 1 ppm/°C on request. Very low noise of less than -30 dB and voltage coefficients of less than 0.1 ppm/V contribute to the excellent performance of these devices.

The Vishay Thin Film PR100 is packaged in a 1.6 mm-wide case with a 1 mm pitch. It is rated for a resistance range of 100 ohms to 200 kilohms and a working voltage of 35 V. In a 1.85 mm-wide case, the PR135 features a 1.35 mm pitch, a resistance range of 100 ohms to 300 kilohms, and a working voltage of 75 V. Finally, the PR182 occupies a 3 mm wide case with a 1.82 mm pitch and is rated for a resistance range of 100 ohms to 1 megohm and a working voltage of 100 V. All three products feature a power rating of 100 mW per resistor at +70 °C and an operating temperature range of -55 °C to +155 °C.

PR series high-precision resistor arrays feature pre-tinned terminations over a nickel barrier. They are available in waffle pack or tape-and-reel packaging.

Samples and production quantities of the new devices are available now, with a lead time of 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Resistor
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account