Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New High-Speed, High-Power Infrared Emitters Are Optimized with 850-nm Wavelength

New Devices Target CMOS Camera Applications, Automotive Night-Vision, and Sensor Systems


infrared emitters

Products mentioned:

TSMG3700
TSHG6200
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

MALVERN, PENNSYLVANIA — July 28, 2004 — Two new infrared emitters aimed at CMOS camera and high-speed IR data transmission applications were launched today by Vishay Intertechnology, Inc. (NYSE: VSH).

The new high-speed, high-radiant power Vishay Semiconductors devices are optimized with an 850-nm wavelength to improve the optical efficiency of CMOS camera illumination systems compared with industry-standard 870-nm emitters. Typical applications for the new devices will include night vision systems and seat occupant sensors in vehicles, for which the 850-nm emitters offer the additional advantage of the low aging rate enabled by their GaAlAs double hetero technology.

These two 850-nm emitters were released today, each with a 20-ns rise time and low 1.8-V maximum forward voltage.

For applications where maximum radiant power and intensity are required, Vishay offers the TSHG6200 in the leaded T 1-3/4 package. Radiant intensity is 180 mW/sr at a forward current of 100 mA, while the 5-mm package provides a ±10° angle of half intensity.

For applications where a device with a wider angle of intensity is preferred, Vishay is offering the TSMG3700 in the miniature PLCC-2 SMD package. This surface-mount emitter combines a ±60° angle of half intensity with a radiant intensity of 10 mW/sr and is easily mounted to printed circuit boards using automatic placement equipment.

Both the TSHG6200 and TSMG3700 are lead (Pb)-free devices.

Samples of the new emitters are available now. Production quantities will be available in Q3 with lead times of 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword