Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New Common-Drain MICRO FOOT® Power MOSFETs Offer On-Resistance Comparable to TSSOP-8 Devices in 81% Smaller Chipscale Package


MOSFETs

Products mentioned:

Si8901EDB
Si8904EDB
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

SANTA CLARA, CALIFORNIA — August 11, 2004 — Two new common-drain, chipscale power MOSFETs that are the industry's first such p-channel and 30-V n-channel devices were announced today by Siliconix incorporated (NASDAQ: SILI), an 80.4%-owned subsidiary of Vishay Intertechnology, Inc. (NYSE: VSH).

Available in the compact 1.6 mm by 2.4 mm chipscale format with a 0.65 mm height profile, the new bi-directional Vishay Siliconix MICRO FOOT® power MOSFET devices are 81% smaller than TSSOP-8 devices, yet provide similar on-resistance values and better thermal performance.

The 20-V Si8901EDB offers ultra-low effective on-resistance of 0.030 Ω, enabled by Vishay's TrenchFET® MOSFET technology. Providing a significant size reduction for lithium-ion and lithium-polymer smart battery packs in portable devices that presently use dual p channel SO-8 or TSSOP-8 MOSFETs, the Si8901EDB can be used to shrink the battery pack circuit considerably or to increase cell volume and hence prolong battery life.

The 30-V Si8904EDB is a compact solution for battery packs used in portable devices with a traditional common-drain n-channel configuration. The Si8904EDB extends Vishay's family of chipscale packaging to include the 30-V value requested by many battery-pack manufacturers today. The new device offers ultra-low on-resistance of 0.0225 Ω, a value similar to that provided by existing TSSOP-8 or SO-8 devices, but in a significantly smaller footprint.

The 20 V Si8901EDB and 30 V Si8904EDB both will be used for battery-protection modules for single-cell LiB and LiP battery packs in cell phones, PDAs, MP3 players, and digital cameras. With their small dimensions, the new MICRO FOOT devices help to prolong standby and talk times by freeing up space that can be used for a larger battery.

Vishay Siliconix MICRO FOOT devices use a solder bump process along with proprietary techniques developed at Siliconix to eliminate the need for an outer package to encase the power MOSFET die, greatly reducing the size of the devices required to switch power and analog signals in cell phones and other handheld systems while also providing a significant reduction in parasitic inductance.

ESD protection is 6 kV for the Si8901EDB and 4 kV for the Si8904EDB. Both devices are fully electrically tested and delivered in tape-and-reel packaging.

Samples and production quantities of the Si8901EDB and Si8904EDB are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

MICRO FOOT is a registered trademark of Siliconix incorporated

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword