VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:New Vishay IHLP Inductors Feature 6.5 mm Height Profile
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/inductors/sales
 

New Vishay IHLP Inductors Feature 6.5 mm Height Profile, Saturation Currents Up to 120 A, and Inductance Values of 5.6 µH, 6.8 µH, 8.2 µH, and 10 µH

New Additions to IHLP Series Have Typical DCR Values Down to 0.47 mΩ

MALVERN, PENNSYLVANIA — September 10, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced four new additions to the IHLP family of low-profile, surface-mount inductors, which now includes standard inductance values ranging from 0.10 µH to 10.0 µH with typical DCR values as low as 0.47 mΩ, saturation currents from 15.5 A to 120 A, and low losses at frequencies up to 5 MHz.

The devices released today provide inductance values of 5.6 µH, 6.8 µH, 8.2 µH, and 10 µH with a tolerance of ±20%.

The patented Vishay Dale IHLP series offers designers higher-performing, power- and space-efficient inductor solutions that measure just 0.508 in. by 0.520 in. by 0.256 in. [12.9 mm by 13.2 mm by 6.5 mm]. Each inductor is packaged in a self-shielded, composite construction that reduces buzz noise to ultra-low levels while meeting military specifications for resistance to thermal shock, moisture, mechanical shock, and vibration.

Target IHLP applications include dc-to-dc conversion and energy storage in end products such as computers, servers, telecom systems, and automotive electronics. In these systems, IHLP devices handle high transient spikes without saturation and at full rated current provide an inductance drop of less than 20% - significantly less roll-off than ferrite materials. All inductors in the IHLP family are 100% lead (Pb)-free and meet RoHS standards.

Samples and production quantities of the new IHLP-5050FD-01 inductors are available now. Lead time for production quantities is seven weeks.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
IHLP Inductors
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account