Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New ESD Protection Diodes in SOD523 Package Provide Working Voltages from 1 V to 12 V and Maximum Clamping Voltages from 9 V to 25 V

Diodes Save Space, Provide Data Line Protection in Portable Electronics


ESD Protection Diodes

Products mentioned:

VESDxx-02V
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

SANTA CLARA, CALIFORNIA — September 17, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of a new ESD protection diode series optimized for space-critical applications with an ultra-small SOD523 (SC79) package measuring 0.8 mm by 1.6 mm by 0.6 mm.

Intended to provide ESD protection for data lines in mobile phone handsets and accessories, cordless phones, laptop computers, PDAs, digital cameras, modems, MP3 players, and other compact, handheld electronics, the new Vishay Semiconductors VESDxx-02V offers one-line transient protection of 15 kV (air) and 8 kV (contact) as per IEC 61000 4 2.

In addition to meeting the high industry standard for ESD protection required by mobile phone manufacturers, the VESDxx-02V series saves space compared to multi-line arrays while giving designers the flexibility to add protection for sensitive electronics on compact circuit boards exactly where it is needed.

The new diode series offers designers a choice of five working voltage values ranging from 1 V to 12 V and maximum clamping voltages from 9 V to 25 V. Low leakage current helps to prolong battery life.

The five devices released today are packaged in a plastic case with a UL 94 V 0 flammability rating and are specified for an operating temperature range of -40 °C to +125 °C. They are available for delivery in tape-and-reel packaging.

Samples and production quantities of the new VESDxx-02V ESD protection diodes are available now with lead times of 8 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword