VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:Vishay's New FC Thin Film Chip Resistors
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/resistors-discrete/thin-film/sales
 

Vishay's New FC Thin Film Chip Resistors Avoid Roll-Off at Frequencies Over 100 MHz, Offer TCR Values Down to ±25 ppm/°C

New Resistors Are Available in Industry-Standard Sizes Down To 0402

MALVERN, PENNSYLVANIA — September 22, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced the release of the new FC series of high-frequency chip resistors, which avoid roll-off even at frequencies over 100 MHz and are available in a range of standard case sizes, including the very compact 0402.

The new Vishay Thin Film FC chip resistors are intended for use in low-noise amplifiers, precision voltage dividers, attenuation circuitry, and line termination applications in fixed telecom and military/aerospace systems requiring fast-response, high-frequency circuitry. High-frequency performance data is provided on the FC product data sheet to help designers choose the best component for their designs, and represents an industry-first capability for this device type.

Designed with low internal reactance, as represented by the capacitance and inductance of the terminations and substrate, the new FC resistor chips function over a very high frequency range. A special laser edge-trimming process allows for precision tolerances down to 0.1%, and resistance values for the chip resistors ranges from 10 Ϋ to 1000 Ϋ, depending on case size. The FC chip resistors offer low TCR values down to ±25 ppm/°C for devices with resistance ratings greater than 50 Ϋ.

Available in the industry's smallest standard formats, including 1206, 1005, 0805, 0603, 0505, and 0402, FC series chip resistors eliminate the need for customizing high-frequency devices or for tuning circuits to the appropriate frequency. As a result, designers have greater flexibility in choosing an off-the-shelf, easy-to-integrate solution that meets the performance demands of high-frequency circuitry.

Each chip resistor features a high-purity (99.6%) alumina substrate and a passivated nichrome resistive layer. Terminations for the FC devices comprise a gold or SN 60 solder over a nickel barrier. All of these devices are rated for stability of 500 ppm/°C over 2000 hours at +70 °C and for an operating temperature range of -55 °C to +125 °C.

Samples and production quantities of the new devices are available now, with a lead time of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Thin Film Chip Resistors
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account