VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:Vishay Tedea-Huntleigh Shear Beam Load Cells Have Nominal Accuracy of ± 0.010 % of Applied Load
For more information:
Media contact: e-mail andrew.post@vishay.com
Sales contact: http://www.vishay.com/load-cells/sales
 

Vishay Tedea-Huntleigh Shear Beam Load Cells Have Nominal Accuracy of ± 0.010 % of Applied Load

Low-profile 3520 range is suited to weighing equipment and industrial applications

MALVERN, PENNSYLVANIA — November 17, 2004 — Vishay Intertechnology, Inc. (NYSE: VSH) announces that the Vishay Tedea Huntleigh 3520 range of shear beam load cells, part of the Vishay Transducers product portfolio, targets low-profile floor scales, pallet scales, and other trade or industrial process and weighing applications. The 19-mm-high load cells save space and enhance the appearance of end products. Stainless steel construction allows easy cleaning and provides high resistance to corrosion. The units are also fully sealed to meet IP67 standards.

Nominal accuracy is up to ± 0.010 % of applied load, with special design features to ensure high thermostability and thereby safeguard accuracy throughout wide temperature fluctuations. The 3520 range also features six-wire cable with two sensing wires, which eliminates measurement inaccuracies due to voltage drops across cables and other interconnection losses. Each unit is supplied with three meters of polyurethane-sheathed, floating-screen cable.

The 3520 range carries approvals for many applications, including OIML (International Organization of Legal Metrology) R60 approval for trade weighing equipment with up to 6000 divisions, and hazardous area approval to ATEX 94/9/EC category EEx ia IIC T6 for explosive atmospheres. This includes the most explosive atmospheres containing hydrogen or acetylene, in which the 3520 load cell is certified for use at temperatures up to +85 °C.

Electrical characteristics include 10 V recommended excitation voltage, with output sensitivity 2 mV/V implying a full-scale output signal of 20 mV. Up to 15 V excitation voltage may be applied.

The compensated operating temperature range for the 3520 load cells is -10 °C to +40 °C (safe operating range is -30 °C to +80 °C). The 3520 family covers the capacity range from 500 kg to 2000 kg. The cells offer robust resistance to shock or side loading, and also deflect less than 0.4 mm at rated capacity.

Vishay Transducers is a division of Vishay Measurements Group. Vishay Measurements Group develops, manufactures, and markets a broad range of sensors for a wide variety of test and measurement applications. These include electrical resistance strain gages for both stress analysis testing and transducer manufacturing applications, instrumentation, hybrid strain gage assemblies and transducers for OEM applications and certified load cells for electronic scales and other weighing applications. Vishay Measurements Group is part of Vishay Intertechnology.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
 
About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account