Searching . . .
About VishayAwardsBrandsCareersContactsEthicsInvestor RelationsProduct NewsTerms and ConditionsTrade Shows

< Back  

For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

Vishay's New Dual High-Voltage Schottky Rectifiers Feature Industry-Best 200-V Reverse Voltage and 20-A Forward Current


Rectifiers

Products mentioned:

MBR
For more information:
Media contact -  Bob Decker, Wall Street Communications
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@wallstcom.com

Sales contact: 

MALVERN, PENNSYLVANIA - November 17, 2004 - Vishay Intertechnology, Inc. (NYSE: VSH) today announced three new dual high-voltage Schottky rectifiers offering a 200-V reverse voltage - the highest available voltage for a silicon Schottky rectifier - a 20-A forward current rating, and a high maximum operating junction temperature of 175 °C.

Outperforming 200-V forward voltage Schottky rectifiers built on silicon carbide technology at a fraction of the cost, these new silicon-based devices are designed for secondary rectification of ac-to-dc and dc-to-dc converters with outputs up to 48 V, as well as freewheeling and polarity protection applications. Package options are the TO-220AB (MBR20H200CT), isolated TO-220AB (MBRF20H200CT), and TO-262AA (MBRB20H200CT-1).

With a low typical forward voltage drop of 0.65 V at 10 A and 125 °C, small 1-mA maximum reverse leakage current at 125 °C, and high 290-A forward surge current per leg, these new Schottky rectifiers have been optimized for 50-W to 250-W power supply applications. They also feature a large peak non-repetitive reverse surge energy of 20 mJ at 8/20 μs per leg.

The new rectifiers provide a negligible reverse recovery time, which, combined with their low forward voltage, improves power efficiency and reduces heat in end products that include the power supplies of desktop and notebook PCs, servers, telecommunication exchangers, HDTVs, and other SMPS devices with high power outputs.

All three devices feature a dual chip, common cathode configuration and maximum operating junction temperature of 175 °C.

Samples and production quantities of the new MBR20H200CT (TO-220AB), MBRF20H200CT (ITO-220AB), and MBRB20H200CT-1 (TO-262AA) Schottky rectifiers are available now, with lead times of six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay's product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

Contact UsSales, Technical Questions...Contact Us
Buy Now Check Distributor Stock Part Number/Keyword