VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:New Dual High-Voltage Schottky Rectifiers
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/diodes/rectifiers/sales
 

Vishay's New Dual High-Voltage Schottky Rectifiers Feature Industry-Best 200-V Reverse Voltage and 20-A Forward Current

MALVERN, PENNSYLVANIA - November 17, 2004 - Vishay Intertechnology, Inc. (NYSE: VSH) today announced three new dual high-voltage Schottky rectifiers offering a 200-V reverse voltage - the highest available voltage for a silicon Schottky rectifier - a 20-A forward current rating, and a high maximum operating junction temperature of 175 °C.

Outperforming 200-V forward voltage Schottky rectifiers built on silicon carbide technology at a fraction of the cost, these new silicon-based devices are designed for secondary rectification of ac-to-dc and dc-to-dc converters with outputs up to 48 V, as well as freewheeling and polarity protection applications. Package options are the TO-220AB (MBR20H200CT), isolated TO-220AB (MBRF20H200CT), and TO-262AA (MBRB20H200CT-1).

With a low typical forward voltage drop of 0.65 V at 10 A and 125 °C, small 1-mA maximum reverse leakage current at 125 °C, and high 290-A forward surge current per leg, these new Schottky rectifiers have been optimized for 50-W to 250-W power supply applications. They also feature a large peak non-repetitive reverse surge energy of 20 mJ at 8/20 µs per leg.

The new rectifiers provide a negligible reverse recovery time, which, combined with their low forward voltage, improves power efficiency and reduces heat in end products that include the power supplies of desktop and notebook PCs, servers, telecommunication exchangers, HDTVs, and other SMPS devices with high power outputs.

All three devices feature a dual chip, common cathode configuration and maximum operating junction temperature of 175 °C.

Samples and production quantities of the new MBR20H200CT (TO-220AB), MBRF20H200CT (ITO-220AB), and MBRB20H200CT-1 (TO-262AA) Schottky rectifiers are available now, with lead times of six weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Rectifiers
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account