VishayOne of the world's largest manufacturers of discrete semiconductors and passive components
Vishay ProductsVishay ProductsCompany InfoCompany InfoCompany Info
Company Info:Press Room:2004 Releases:Vishay's New High-Speed 10 MBd Optocouplers
For more information:
Media contact: e-mail bob.decker@wallstcom.com
Sales contact: http://www.vishay.com/optocouplers/sales
 

Vishay's New High-Speed 10 MBd Optocouplers in Single- and Dual-Channel Configurations Feature +100 °C Capability in SOIC-8 Package

SANTA CLARA, Calif. - December 17, 2004 - Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new series of 10 MBd optocouplers in an SOIC-8 packaged rated for operating temperatures up to +100 °C.

The new SFH67xxT optocouplers feature a reinforced-insulation construction combining a highly efficient input LED with an integrated optical photodiode IC detector optimized for applications requiring high data rates such as communication bus lines, high-speed A/D and D/A converters, digital control power supplies, industrial controller I/O interfaces, and scan driver IC interfaces for plasma display panels.

Along with a typical speed of 10 MBd and operating temperature range of −40 °C to 100 °C, the new optocouplers from Vishay Semiconductors feature CMR values up to 10,000 V/µs, typical pulse-width distortion (PWD) of 2.9 ns, typical propagation delay (tPHL) of 50 ns, and fast rise and fall times of 23 ns and 7 ns, respectively.

Vishay’s 10 MBd optocouplers deliver improved output leakage current performance thanks to their NMOS open drain output structure. In addition, they provide a higher isolation replacement for signal isolation transformers, as well as noise immunity and diminished electromagnetic interference by reducing potential ground loops in electronic equipment.

The six new optocouplers are available in a standard SOIC 8 package with reinforced insulation per IEC60950 2.10.5.1 and eight pure tin leads. Three are configured with a single channel and three with dual channels, with each configuration offering a choice of CMR values of 100 V/µs, 5,000 V/µs, or 10,000 V/µs. The single-channel devices also feature an enable function on the seventh pin for strobing the detector.

10 MBd High-Speed Optocouplers: Summary Table

Part

CMR (V/µs)

Configuration

Package Type

SFH6745T

100

Single-channel

SOIC-8

SFH6746T

5,000

Single-channel

SOIC-8

SFH6747T

10,000

Single-channel

SOIC-8

SFH6755T

100

Dual-channel

SOIC-8

SFH6756T

5,000

Dual-channel

SOIC-8

SFH6757T

10,000

Dual-channel

SOIC-8

The SFH67xxT optocouplers interface easily with most standard logic families and reduce design cycle time by simplifying overall system noise design considerations.

Samples of the new 10 MBd optocouplers are available now with lead times of six to eight weeks for larger orders. Production quantities will be available in December 2004.

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, transistors, and optoelectronics and selected ICs) and passive electronic components (resistors, capacitors, inductors, sensors, and transducers). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, and medical markets. Its product innovations, successful acquisition strategy, and ability to provide "one-stop shop" service have made Vishay a global industry leader. Vishay can be found on the Internet at http://www.vishay.com.

###

 
Optocouplers
 

Products mentioned:

 

This release in:

About Vishay
Brands
Careers
Contacts
Ethics
Investor Relations
Product News
2008 releases
2007 releases
2006 releases
2005 releases
2004 releases
*2003 releases
*2002 releases
*2001 releases
*2000 releases
*1999 releases
Trade Shows
Vishay History
Products A-Z
Company Info:   Press ·  Investors ·  Contacts ·  More...
Privacy & Legal · Your Account